I use JN-AN-1135 project as template.
There is presented Tunneling cluster between ESP and Plug Meter node.
I want to implement it on the second Plug Meter node with another IEEE/MAC.
But when i do that i have expected problems with an Application Level Security.
In fact I do not need any security in my project, i need only I need only a tunneling cluster (mechanizm which can transmit long payload throw the ZigBee network).
Can anyone help me?
Hi Arthur,
Could you please check the ZigBee PRO Stack User Guide JN-UG-3048?
5.7 Implementing ZigBee Security
5.7.2 Application-level Security Set-up
If security is enabled in a ZigBee network then network-level security is always used, while application-level security is optional. Security is enabled on a node via the device parameter Security Enabled in the ZPS Configuration Editor.
http://www.nxp.com/documents/user_manual/JN-UG-3048.pdf
Hope it helps.
Regards,
Mario