Hi,
I am newbie to the Metrowerks and I would like to create XML files from .mcp files. There is an option File->export project to as XML file.
But here is the situation. I have a main project which includes several (around 50) sub projects. If I use the IDE, I need to open each and every project and export it as XML file. Instead I am looking for an option from command line to generate XML files for a given .mcp file.
It looks like the exported XML file from IDE doesn't include the header files. I read somewhere in forum , the header files can be extracted from .cdt files, but no procedure found
Basically I need this option to compare for addition/removal of source/header files for each version of the project (Note: Main project contains several sub projects).
Please let me know for any other options using IDE or command line tools.
Thanks,
Ram