P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools, debug probes, and production programmers
The chip is on an Adapt9S12D board from technological arts, I am using the
program PROG12Z - Flash Programmer, I have loaded every Freescale 9S12DP512
module in your libraries and always get an issue when I try programming
starting at base address 00000. I get a warning saying "All S record addresses
not in range or module."The error I receive is "No data to program" "Invalid
addresses in srecord block from $0000C000 to $0000C01F. I have reloaded the
modules starting with the base address of C000 and then programmed it without
error but I get the same warning and this time it states the invalid address
range at D000 to D01F. I think my real issue may be not having the right module
for my chip. The puzzling thing is that I am programming a replacement board
from an old project that was at one point programmed with a cyclone pro so
There should be a way to do it because it was done at one point. Any
suggestions would be very helpful. |
|
|
|
|