Hi I just searched for new software and it found what I think was some gdb debug update (didnt pay much attention as I just expect updates to work) and now debugging is impossible... KDS is crashing
Every time i go to debug it shows
Appears something is crashing and changing my debug configuration so I have to go select the correct debug config, so I do that then I get
So I have to kill it via task manager
Im literally using this program 10 hours a day, I cant use it any more, i spend all day doing the above since that update.
Also, when I go to debug with freertos now every time i try to break it just stops here so its now impossible to debug anything:
void vPortYield( void )
{
/* Set a PendSV to request a context switch. */
*( portNVIC_INT_CTRL ) = portNVIC_PENDSVSET;
/* Barriers are normally not required but do ensure the code is completely
within the specified behaviour for the architecture. */
__asm volatile( "dsb" );
__asm volatile( "isb" );
}
/*---
I just reinstalled everything from scratch, when you go to do the update that kills it it shows this
but still does the update... and kills it...
Hi Carl,
the 'handshake_failure' is because of SourceForge needing a new Java certificate (see GNU ARM Eclipse plug-ins: Received fatal alert: handshake_failure ). KDS is using its own VM, so installing the needed certificates is not what I recommend. Instead, what works for me is to download the zip file from the Releases (Releases · gnuarmeclipse/plug-ins · GitHub ) page and then use that zip file with Help > Install New Software.
I hope this helps,
Erich
PS: I'm very happy with the GNU ARM Eclipse plugins.
So I did it all again without that pe update and its fine now... 65Mb pe micro update destroys KDS debug capablities.