Hello,
Serial/SPI NAND Flash offers advantages for lower memory densities, but it's not clear in the datasheet if it supports Serial/SPI NAND? eMMC is supported and desirable because of the error management built inside. Since Serial/SPI NAND can be used reliably in systems that provide bad-block management and error-correction algorithms, it looks like I have to this management in the i.MX6ULL.
Does the MX6ULL support Serial/SPI NAND with 8-bit ECC?
Thanks in advance,
Scott
Hi Scott
supported serial memory devices, such as EEPROM and serial flash, using the SPI,
Serial/SPI NAND not supported.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------