Is i.MX6 able to connect 2 small LCD (QVGA) panel?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is i.MX6 able to connect 2 small LCD (QVGA) panel?

531 Views
t-iishii
Contributor II

Hi community,

Out customer plan to use 2 small LCD. Pixel size is a QVGA.

Input signal of LCD panel is a 8-bit sequential data like this.

       |<-----------  960 clock/line ------------------------------->

PCLK   _|~|_|~|_|~|_|~|_|~|_|~|_|~|_|~|_|~|_|~|_|~|_|~|_|~|_|~|_|~|_|~ 

D[7:0] _X_R_X_G_X_B_X_R_X_G_X_B_X_R_X_G_X_B_X_R_X_G_X_B_X_R_X_G_X_B_X

To connect 2 different LCD panel, is I.MX must use more than 1ch LVDS I/F?

If so, LVDS can output RGB sequential data format like this?

Best regards,

Ishii.

Labels (3)
0 Kudos
Reply
2 Replies

437 Views
t-iishii
Contributor II

Hello Igor

Thank you for your quick response.

Best regards,

Ishii.

0 Kudos
Reply

437 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

>To connect 2 different LCD panel, is I.MX must use more than 1ch LVDS I/F?

yes

ldb module supports only data mapping given in Table 39-6,Table 39-7 SPWG/JEIDA Data Mapping

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
and example can be found on p.16 sect6.3 Bit Mapping & Interface Definition HSD100P HannStar LCD datasheet

https://community.freescale.com/message/331832#331832

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply