LS1021A Reset Reason

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021A Reset Reason

1,441 Views
greghuber
Contributor II

Other than the WDOG, does the LS1021A have any 'reset reason' registers similar to the iMX.6? We have a small system that just reboots every 4-5 minutes but only when when idle. We have disabled the internal WDOG with no effect.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,234 Views
Pavel
NXP Employee
NXP Employee

Look at the Reset Request Status Register (DCFG_CCSR_RSTRQSR1).

 

See also the Reset Control Register (DCFG_CCSR_RSTCR)


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply