I am trying to booting profile all branches kernel in ep8248e board which has Freescale MPC8248 processor.
Kernel booting is failing when CONFIG_PROFILE_ALL_BRANCHES is enabled in MPC8241 processor.
It gets stuck after Finalizing device tree ....
Memory <- <0x0 0x8000000> (128MB)
zImage starting: loaded at 0x00900000 (sp: 0xf0001d20)
Allocating 0x8d2838 bytes for kernel ...
gunzipping (0x00000000 <- 0x0090e000:0x00ca6378)...done 0x880dc0 bytes
Linux/PowerPC load:
Finalizing device tree... flat tree at 0xcb3300
Please specify which Linux BSP you are using, and where it was obtained from?
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Linux BSP is build from git://git.freescale.com/ppc/sdk/linux.git
Git tag checkout : fsl-sdk-v1.4
I do not see MPC8248 processor listed as supported in SDK 1.4