Ethernet Independent mode in DPAA QorIQ processors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet Independent mode in DPAA QorIQ processors

Jump to solution
1,402 Views
talhaimran
Contributor II

I am implementing Ethernet independent mode in DPAA, Does independent DPAA mode require FMan ucode?

1 Solution
1,046 Views
bpe
NXP Employee
NXP Employee

Yes, FMan microcode is required for FMan Independent mode.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,047 Views
bpe
NXP Employee
NXP Employee

Yes, FMan microcode is required for FMan Independent mode.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,046 Views
talhaimran
Contributor II

Thanks Paton. One more thing I am confused about is the MDIO interface present in the Fman controller. If we use the internal MDIO interface for each MAC we access the MDIO registers of SERDES which automatically reports the the AN as complete and link status as up, even if no cable is attached to port. While if we use the external MDIO interface and access the PHY for same MAC then we access the standard PHY register which reports correct link and auto negotiation status. So what link status are the SERDES MDIO registers referring to?

0 Kudos
Reply