Hi All,
I am facing some problem with imx6q sabrelite u-boot.It constantly shows error raise: Signal # 8 caught.
U-Boot 2016.03 (Dec 21 2016 - 14:54:21 +0530)
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
Reset cause: POR
Board: SABRE Lite
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB
raise: Signal # 8 caught
raise: Signal # 8 caught
raise: Signal # 8 caught
raise: Signal # 8 caught
raise: Signal # 8 caught
...
I think this problem is because of some incorrect boot argument.Kindly suggest how to reset boot args saved in SPI.
Thanks
Solved! Go to Solution.
Hi,
Yes it is normal since you set env to mmc in this U-Boot configuration.
Instead, you need to enter the following commands:
=> sf probe
=> sf erase 0xc0000 0x2000
Regards,
Gary
Hi,
I tried a custom u-boot with CONFIG_ENV_IS_IN_MMC macro.
Now I am able to access u-boot prompt,but while saving new boot args it gives a error.
Saving Environment to MMC...
MMC: no card present
!MMC init failed
Hi,
Yes it is normal since you set env to mmc in this U-Boot configuration.
Instead, you need to enter the following commands:
=> sf probe
=> sf erase 0xc0000 0x2000
Regards,
Gary
Hi,
I am not able to access uboot prompt.
This error started after I updated boot args.
Hi,
In that case, I suggest you re-build a custom U-Boot that doesn't read the environment from SPI NOR:
u-boot-imx6/boundary.h at boundary-v2016.03 · boundarydevices/u-boot-imx6 · GitHub
Then I would use that procedure to boot this binary:
Unbricking a Nitrogen6X or Sabre Lite i.MX6 board - Boundary Devices
Then you should get U-Boot prompt again.
Hope this helps.
Regards,
Gary
Hi,
Can you access the U-Boot prompt?
If so, please enter:
=> env default -a
=> saveenv
Did this error occur after a U-Boot upgrade?
Regards,
Gary