iMX6 to DDR3: clock length calculation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 to DDR3: clock length calculation

Jump to solution
723 Views
ilariogottardel
Contributor II

Hello,

we are designing a board with i.MX6 Quad and DDR3 and we are in doubt about how to calculate clock length.

As you can see in the image below, we have tracks that go from CPU to RAM chips, and than they go on to the termination resistor (highlighted with the arrows).

Immagine.png

Are those tracks to be counted in the clock length? Or should we only count the path from CPU pad to RAM pad?

Thank you very much

Have a nice day

Ilario Gottardello

Labels (1)
1 Solution
586 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ilario

right, one should count the path from CPU pad to RAM pad.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
587 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ilario

right, one should count the path from CPU pad to RAM pad.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply