MKM14Z128ACHH5R vs MKM14Z128CHH5R

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKM14Z128ACHH5R vs MKM14Z128CHH5R

514 Views
jonathanpittock
Contributor I

Hi,

The MKM14Z128CHH5R is not recommended for new designs and a new part is offered as its replacement, the MKM14Z128ACHH5R.  Can anyone explain the difference and the meaning of the 'A' suffix.  Would this alternative part have any major impact on designs using the original MKM14Z128CHH5R?

Thanks


Jon

0 Kudos
Reply
1 Reply

368 Views
MarMi
NXP Employee
NXP Employee

Hi Jon,

parts with 'A' suffix have the following improvements:

Description

MKMxxZxxAC ('A' suffix)

MKMxxZxxC (original)

RTC 1Hz clock output edge generation with fine resolution

on both rising edge to rising edge and falling edge to falling edgeon rising edge to rising edge only

Typical internal voltage reference temperature drift across full temperature range 

10 ppm/°C  
(ICOMPEN control bit introduced enabling second order curvature compensation)
18 ppm/°C  
(ICOMPEN control bit missing)

errata 6665: limitation of the device operating range

fixedpresent

Kind regards,

Martin M.

0 Kudos
Reply