Can we use two x16 DDR3L SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use two x16 DDR3L SDRAM

530 Views
gokulkrishnan
Contributor III

Hi,

I am in need of using two x16 DDR3L SDRAM along with the T1042 processor. How should I go about this. Can i just connect the 32 data bits and the required ECC and MDQS, MDM signlas or is there a special way i should do them!

Regards 

Gokul

Labels (1)
0 Kudos
Reply
1 Reply

413 Views
Bulat
NXP Employee
NXP Employee

Yes, you need to connect your SDRAMs to MDQ[0..31] data and corresponding MDQS/MDM (and ECC) signals for 32-bit DDR interface. DDR_DDR_SDRAM_CFG[DBW] register controls data bus width.

Regards,

Bulat

0 Kudos
Reply