hi nxp fae,
In the file of "i.MX_Linux_Release_notes.pdf(Rev. L4.1.15_2.0.0-ga)" has a "e-ink-waveform-firmware.bin".
Table 7. Controlled access packages
Is the "eink-waveform-firmware-1.0.1.bin" a set of *.fw or not ?
what's the mean "REGAL/-D waveform "? Is a advanced feature?
thanks.
Solved! Go to Solution.
Q. Is the "eink-waveform-firmware-1.0.1.bin" a set of *.fw ?
A. Yes.
Q. what's the mean "REGAL/-D waveform "? Is a advanced feature?
A. Yes, this is a set of advanced features, mostly related with partial page refresh.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Q. Is the "eink-waveform-firmware-1.0.1.bin" a set of *.fw ?
A. Yes.
Q. what's the mean "REGAL/-D waveform "? Is a advanced feature?
A. Yes, this is a set of advanced features, mostly related with partial page refresh.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------