can the MPXx6250A be used as a vacuum sensor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can the MPXx6250A be used as a vacuum sensor?

522 Views
rodschulz
Contributor I

I have an automotive application and want to know if the MPXx6250A can be used as a vacuum sensor?  My vacuum levels are ~ 14inHg to 24inHg.

Labels (1)
0 Kudos
1 Reply

252 Views
david_diaz
NXP Employee
NXP Employee

Hello Rod,

Thank you for writing.

As we know, the MPXx6250A is an absolute pressure sensor. The absolute pressure is the difference between the pressure at a given point and the absolute zero of pressure or a perfect vacuum. In other words: pressure is applied on Port P1 of the sensor while the Port P2 of the sensor is a vacuum sealed reference.

The pressure range of the MPXx6250A is from 20 kPa to 250 kPa (5.906 inHg - 73.825 inHg), which is within the levels mentioned.

I assume the device is useful for your application.

 

Please let me know if I understood your question.

Best Regards,

David

0 Kudos