Hi
in the datasheet of iMX6 is written: VDD_ARM_IN and VDD_SOC_IN may be supplied from the same source.
in the datasheet iMX7 is missing this kind of iformation.
Is it possible to supply both rails (VDD_ARM and VDD_SOC) from the same source?
Regards
Lubomir
Hi Yuri,
thanks for answer.
If the voltage VDD_ARM is set to 1.1V then iMX7 can operate with max frequency 1GHz.
1.1V is still in recommended range for VDD_SOC.
I think that typ 1.1V is ok for VDD_SOC rail.
What is your opinion?
Regards
Lubomir
Hello,
Generally - yes, both suppliers may be provided from the same source,
but please pay attention on operating range specs in Table 9 of i.MX7 Datasheet(s).
Allowed voltage ranges for different modes are not the same for VDD_ARM_IN and VDD_SOC_IN.
The same source may be applied for run mode at 800 MHz and below.
http://cache.nxp.com/files/32bit/doc/data_sheet/IMX7DCEC.pdf?pspll=1
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct
Answer button. Thank you!
------------------------------------------------------------------------------