Booting T1040RDB.
I am using "QorIQ-SDK-V2.0-20160527-yocto". I am trying to build u-boot image for T1040rdb reference board.
./fsl-setup-env -m t1040d4rdb
bitbake -f u-boot
Tried to flash u-boot.bin from tmp/deploy/images.
U-Boot 2016.012.0+ga9b437f (Oct 04 2016 - 15:33:07 -0700)
CPU0: T1022, Version: 1.1, (0x85210211)
Core: e5500, Version: 2.1, (0x80241021)
Single Source Clock Configuration
Clock Configuration:
CPU0:1400 MHz, CPU1:1400 MHz,
CCB:600 MHz,
DDR:600 MHz (1200 MT/s data rate) (Asynchronous), IFC:150 MHz
QE:300 MHz
FMAN1: 600 MHz
QMAN: 300 MHz
PME: 300 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Reset Configuration Word (RCW):
00000000: 0c0c000e 0e000000 00000000 00000000
00000010: 66000002 00000012 ec027000 01000000
00000020: 00000000 00000000 00000000 00032810
00000030: 00000300 00049680 00000000 00000000
I2C: ready
Board: T1022D4RDB
Board rev: 0xff CPLD ver: 0xff, vBank: 7
SPI: ready
DRAM: Initializing....using SPD
Ctrl 0 DIMM 0: is not a DDR4 SPD.
Error: No valid SPD detected.
*** failed ***
initcall sequence effccd9c failed at call eff4d5dc (err=1)
### ERROR ### Please RESET the board ###
Any inputs whats happening?
Thanks
Vijay
Hi,
Even I too did the same problem. Now how can I download the working u-boot (SDK 1.6) on to the T1040RDB again ?
Best regards
Prashanth
I am using T1040DB Rev B. what SDK do you recommend and link for the same
Thanks
Vijay
Please study the table at the link above
Regards,
Platon
You seem to be trying to boot an SDK 2.0 u-Boot image on an unsupported, pre-D4 board which has another type
DDR SDRAM and therefore fails. Use the SDK release that supports your hardware version:
Have a great day,
Platon