The Power Consumption for i.MX6 Quad PLUS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The Power Consumption for i.MX6 Quad PLUS

Jump to solution
1,786 Views
yuuki
Senior Contributor II

Dear all,

We use i.MX6Quad now.
We want to use i.MX6Quad PLUS next.


We want to confirm power consumption for i.MX6Quad PLUS.

(We want to compare Quad PLUS with Quad)
However, we were not able to find this in a Web site.


May I have a power consumption application notes for i.MX6Quad PLUS?

Best Regards,
Yuuki

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
862 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Yuuki,

There is not an Application Note covering Power Consumption for the i.MX6QP yet, but the recommendation is to use the Application Note for the i:MX6Q as reference in the meantime.

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf 

Power Consumption for the i.MX6QP is expected to be higher than the i.MX6Q but not by much. The PF0100 should suit the i.MX6QP needs after the specs were updated for SW2 from 2A to 2.5A.

I hope this information helps!

Regards,

View solution in original post

0 Kudos
Reply
1 Reply
863 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Yuuki,

There is not an Application Note covering Power Consumption for the i.MX6QP yet, but the recommendation is to use the Application Note for the i:MX6Q as reference in the meantime.

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf 

Power Consumption for the i.MX6QP is expected to be higher than the i.MX6Q but not by much. The PF0100 should suit the i.MX6QP needs after the specs were updated for SW2 from 2A to 2.5A.

I hope this information helps!

Regards,

0 Kudos
Reply