I am having problems with flashing my target with a LPCLink2 programmer. Occasionally, when flashing from the command line, the flashing fails with
1
Ni: LPCXpresso RedlinkMulti Driver v8.2 (Jun 30 2016 17:49:22 - crt_emu_cm_redlink build 723)
Pc: ( 0) Reading remote configuration
Pc: ( 5) Remote configuration complete
Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(38). Invalid probe index.'
Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(38). Invalid probe index.'
Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(38). Invalid probe index.'
Nc: probe unbooted? no core 0?
Ed:02: Failed on connect: Ee(38). Invalid probe index.
Et:31: No connection to emulator device
Pc: (100) Target Connection Failed
This error might show up with one user account while it still works from another one, on the same machine, with the same target.
I seem to not be able to repeat the problem when running from LPCXpresso GUI, but this might be just a statistical fluke. The failures seem to come "clustered", i.e. if it does not work once, it probably will not work if I retry, either. This makes figuring this out more difficult.
Launching the GUI is not a possible solution here, as I am building up an automated test setup. The command line I use for flashing is generated by the LPCXpresso GUI.
The machine is an Ubuntu 16.04, x86_64. LPCXpresso is version v8.2.0 [Build 647] [2016-07-18].
Any suggestions on what I could try?
thank you in advance,
kalle
Solved! Go to Solution.
What actually is the command line that you are passing in? Are you passing in a probe index, if so, do you see the same issue if you remove this parameter?
And I presume you are booting the probe first, as per: Booting LPC-Link2
PS : The following might be useful background if you haven't seen it already: https://community.nxp.com/thread/389139
Regards,
LPCXpresso Support
What actually is the command line that you are passing in? Are you passing in a probe index, if so, do you see the same issue if you remove this parameter?
And I presume you are booting the probe first, as per: Booting LPC-Link2
PS : The following might be useful background if you haven't seen it already: https://community.nxp.com/thread/389139
Regards,
LPCXpresso Support
That booting of the flasher seems to have been it. I had missed that documentation it completely... Thanks for the patience :smileyhappy: