The creation of such a PBL image requires:
the QorIQ Configuration Suite (QCS) PBL tool.
QCS can be downloaded from http://www.freescale.com/QCS
Install QCS and review its documentation before proceeding
Not Found
The requested URL /QCS was not found on this server.
Additionally, a 500 Internal Server Error error was encountered while trying to use an ErrorDocument to handle the request.
Freescale Linux SDK for QorIQ Processors |
The best way to get a QCVS update is to use the update site. Which SoC are you using?
B4860QDS 64-bit
For power architecture, available update site over CW is FSL PA QCVS - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win. This should be use from CodeWarrior, Help > Install New Software. When/if updates are available, this is the main update channel.
Adrian
NXP QCVS tool can be downloaded using the following page:
Downloading requires registration on NXP.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------