Manual is wrong on QCS download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Manual is wrong on QCS download

1,175 Views
chandramills
Contributor I

Test Procedure

The creation of such a PBL image requires:

  1. a known working RCW, taken from the QorIQ SDK release.
  2. the QorIQ Configuration Suite (QCS) PBL tool.

    QCS can be downloaded from  http://www.freescale.com/QCS
    Install QCS and review its documentation before proceeding
  3. a U-boot image for booting from eSPI flash, SD Card or NAND flash, built from the QorIQ SDK release.

Not Found

The requested URL /QCS was not found on this server.

Additionally, a 500 Internal Server Error error was encountered while trying to use an ErrorDocument to handle the request.

Freescale Linux SDK for QorIQ Processors

0 Kudos
4 Replies

764 Views
addiyi
NXP Employee
NXP Employee

The best way to get a QCVS update is to use the update site. Which SoC are you using?

0 Kudos

764 Views
chandramills
Contributor I

B4860QDS 64-bit

0 Kudos

764 Views
addiyi
NXP Employee
NXP Employee

For power architecture, available update site over CW is FSL PA QCVS - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win. This should be use from CodeWarrior, Help > Install New Software. When/if updates are available, this is the main update channel.

Adrian 

0 Kudos

764 Views
Pavel
NXP Employee
NXP Employee

NXP QCVS tool can be downloaded using the following page:

http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-to...

 

Downloading requires registration on NXP.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos