Gpio pin interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gpio pin interrupt

3,694 Views
gvisser
Contributor II

Hello,

I am have a problem with receiving interrupts from the gpio pins.

The problem is that I never seem to receive an interrupt.

I can read the pin an have confirmed that it does change however I do not get an interrupt.

Can someone please advice me what i should do to get the interrupts on the rising and falling edge.

ResetISR()

{

    Chip_SCU_PinMuxSet( 6, 5, (SCU_MODE_MODE_PULLUP | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC0) );

    Chip_SCU_PinMuxSet( 1,14, (SCU_MODE_MODE_PULLUP | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC0) );

}

int main(void)

{

    static const uint32_t        c_controllerPort = 3;

    static const uint8_t        c_controllerPin = 4;

    static const uint32_t        c_responderPort = 1;

    static const uint8_t        c_responderPin = 7;

    bool controllerPin = 0;

    bool responderPin = 0;

    Board_Init();

    Chip_Clock_Enable(CLK_MX_GPIO);

    Chip_GPIO_Init(LPC_GPIO_PORT);

    Chip_GPIO_WriteDirBit(LPC_GPIO_PORT, c_controllerPort, c_controllerPin, false);

    Chip_GPIO_WriteDirBit(LPC_GPIO_PORT, c_responderPort, c_responderPin, false);

    Chip_GPIO_IntCmd(LPC_GPIO_PIN_INT, c_controllerPort, c_controllerPin, GPIOPININT_RISING_EDGE);

    Chip_GPIO_IntCmd(LPC_GPIO_PIN_INT, c_controllerPort, c_controllerPin, GPIOPININT_FALLING_EDGE);

    Chip_GPIO_IntCmd(LPC_GPIO_PIN_INT, c_responderPort, c_responderPin, GPIOPININT_RISING_EDGE);

    Chip_GPIO_IntCmd(LPC_GPIO_PIN_INT, c_responderPort, c_responderPin, GPIOPININT_FALLING_EDGE);

    Chip_SCU_GPIOIntPinSel(0, c_controllerPort, c_controllerPin);

    Chip_SCU_GPIOIntPinSel(1, c_responderPort, c_responderPin);

    NVIC_SetPriority(PIN_INT0_IRQn, 1);

    NVIC_SetPriority(PIN_INT1_IRQn, 2);

    NVIC_ClearPendingIRQ(PIN_INT0_IRQn);

    NVIC_ClearPendingIRQ(PIN_INT1_IRQn);

    NVIC_EnableIRQ(PIN_INT0_IRQn);

    NVIC_EnableIRQ(PIN_INT1_IRQn);

    while(true)

    {

        if(controllerPin != Chip_GPIO_ReadPortBit(LPC_GPIO_PORT, c_controllerPort, c_controllerPin))

        {

            controllerPin ^= 1;

        }

        if(responderPin != Chip_GPIO_ReadPortBit(LPC_GPIO_PORT, c_responderPort, c_responderPin))

        {

            responderPin ^= 1;

        }

    }

}

extern "C" void GPIO0_IRQHandler(void)

{

    while(true);

    Chip_GPIO_IntClear(LPC_GPIO_PIN_INT, CUartOverGpio::c_controllerPort, CUartOverGpio::c_controllerPin);

    NVIC_ClearPendingIRQ(PIN_INT0_IRQn);

}

extern "C" void GPIO1_IRQHandler(void)

{

    while(true);

    Chip_GPIO_IntClear(LPC_GPIO_PIN_INT, CUartOverGpio::c_responderPort, CUartOverGpio::c_responderPin);

    NVIC_ClearPendingIRQ(PIN_INT1_IRQn);

}

Labels (1)
Tags (3)
0 Kudos
Reply
4 Replies

1,831 Views
athmesh_n
Contributor IV

 Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 5,(IOCON_DIGMODE_EN | IOCON_MODE_INACT) );
 /* Configure GPIO pin as input */
 Chip_GPIO_SetPinDIRInput(LPC_GPIO, 0, 5);
 /* Enable PININT clock */
 Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_PININT);
 /* Reset the PININT block */
 Chip_SYSCTL_PeriphReset(RESET_PININT);
 /* Configure interrupt channel for the GPIO pin in INMUX block */
 Chip_INMUX_PinIntSel(0, 0, 5);
 /* Configure channel interrupt as edge sensitive and falling edge interrupt */
 Chip_PININT_ClearIntStatus(LPC_GPIO_PIN_INT, PININTCH(0));
 Chip_PININT_SetPinModeEdge(LPC_GPIO_PIN_INT, PININTCH(0));    //working as high edge interrupt for npn sensor
 Chip_PININT_EnableIntHigh(LPC_GPIO_PIN_INT, PININTCH(0));    //int high edge
 /* Enable interrupt in the NVIC */
 NVIC_ClearPendingIRQ(PIN_INT0_IRQn);
 NVIC_EnableIRQ(PIN_INT0_IRQn);
0 Kudos
Reply

1,831 Views
gvisser
Contributor II

Hello,

Thank you for your reply.
I am using the LPC1837FET100 on a custom PCB.
I have looked at the the examples hover I did not manage to get it to work.

Best regards,
Guido

0 Kudos
Reply

1,831 Views
DavidS
NXP Employee
NXP Employee

Hi Guido,

I'm kind of new to LPC products and currently using the new LPCOpen that what I think you are as the API's are slightly different.

I am using LPCOpen_v2.05.  Can you try using new version and the periph_pinint example?

I used my OM13076 (LPC18s37) board to test rising and falling with the SW2 on the board and it works fine.

Attached is my pinint.c with modifications to have both edges working to toggle blue LED.

Regards,

David 

0 Kudos
Reply

1,831 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Could you let us know which LPC product you are using?

There with an example for GPIO group interrupt for LPC4357 product at LPCOpen software (Keil MCB4300 board).

Customer could refer that example as well.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply