Porting u-boot from imx6ul evk board to a custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting u-boot from imx6ul evk board to a custom board

1,411 Views
monicaruiz
Contributor II

Hello,

I am starting to port the BSP from a reference board, in this case imx6ul evk, to my custom board.

As I read, I have to create an entry in boards.cfg file for my own board, but I cannot find this file in my u-boot-imx directory.

Should I create it or where can I find it?

Thanks in advance.

Mónica

Tags (1)
0 Kudos
3 Replies

856 Views
monicaruiz
Contributor II

Hello,

This question has been "assumed answered" but I don't know the reason because there is no answer.

Maybe the question is too much obvious but I cannot find a solution for it so I would be really happy if someone can just guide me with this.

0 Kudos

856 Views
Yuri
NXP Employee
NXP Employee

Hello,

Please refer to the following
U-Boot Migration Example

Recent BSP documentation may be found at


i.MX 6 Series Software and Development Tool|NXP

Regards,

Yuri.

0 Kudos

856 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mónica

please check *.cfg files on below link

uboot-imx.git - Freescale i.MX u-boot Tree

also check attached Porting Guide Chapter 1

Porting U-Boot from an i.MX 6/7 Reference Board to

an i.MX 6/7 Custom Board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos