S12ZVL LIN Phy voltage chatesteristic inTx mode.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVL LIN Phy voltage chatesteristic inTx mode.

443 Views
rajivbandodkar
Contributor II

Hi,

In Knox datasheet, I can find LIN Phy receiver voltage thresholds as under

159571_159571.pngpastedImage_1.png

What about the characteristics in Tx Mode?

Also can you explain the parameters in below table... We are operating at 19.2 K baud.

159570_159570.pngpastedImage_0.png

 

Regards,

Rajiv Bandodkar.

Labels (1)
0 Kudos
1 Reply

271 Views
iggi
NXP Employee
NXP Employee

Hi Rajiv,

Those characteristics are taken from general LIN Specification Package defined by LIN consortium and then standardized by ISO.

www.lin-subbus.org

The LIN specification package you can download here:

http://www.cs-group.de/fileadmin/media/Documents/LIN_Specification_Package_2.2A.pdf 

"For a correct transmission and reception of a bit, it has to be asserted that the signal is available with the correct voltage level (dominant or recessive) at the bit sampling time of the RECEIVER." So, there is no need to specify in Tx mode.

- Rising and falling edge times parameter are clear.

- Not sure what is over-current masking window

Duty cycle is the percentage of one period in which a signal or system is active. The same as with PWM.
Duty cycle - Wikipedia, the free encyclopedia 

Have a great day,
iggi

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos