Hello Champs,
I got unhandled exception error running my RTOS on i.MX502.
In i.MX502 Cortex-A8 cp15 c9 "L2 Cache Auxiliary Control Register",
bit25 is "Write combining disable".
The default is "0 = enables write combine, default"
Is there any case this default setting can cause unhandled exceptions?
BR,
N.Shinozaki
No. Everything should be fine with default settings of cache.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------