Using the ID acceptance filter MSCAN KEA128?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the ID acceptance filter MSCAN KEA128?

Jump to solution
2,579 Views
emilioaronmoyer
Contributor III

Hello,

I'm trying to understand how the id acceptance filter for MSCAN works in KEA128, does any one have an idea of how it works?, how the  CANIDAR0-CANIDAR3, CANIDMR0-CANIDMR3 registers have to be configured? which logical operator is used where comparing the registers with the id read (or,and,etc)? which result will remain after passing all the filters for an id to be accepted?

I have read section 32.4.5 Identifier acceptance filter, but I don't figure it out how it works.

Regards,

Emilio Moyers

Labels (1)
0 Kudos
Reply
1 Solution
2,073 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Emilio,

As you have read section  32.4.5 Identifier acceptance filter in the RM of KEA128, the MACAN receiver is a 5 stage FIFO instead of separate message buffers, there is only one address space for the receiver FIFO, the actual message ID which is received by MSCAN is saved in MSCAN_REIDR0~3 for 29 bits extended ID and MSCAN_REIDR0~1 for 11 bits standard ID.

Regarding the acceptance of filter, there are two bank: fisrt bank and second bank.

The first bank includes the following registers:

MSCAN_CANIDAR0~3

MSCAN_CANIDMR0~3

The second bank includes the following registers:

MSCAN_CANIDAR4~7

MSCAN_CANIDMR4~7

The IDAM bits in MSCAN_CANIDAC define the filter pattern, I copy it here:

"

Identifier Acceptance Mode

The CPU sets these flags to define the identifier acceptance filter organization.

In filter closed mode, no message is accepted such that the foreground buffer is never reloaded.

00 Two 32-bit acceptance filters.

01 Four 16-bit acceptance filters.

10 Eight 8-bit acceptance filters.

11 Filter closed.

"

Assume that you set the IDAM bits as 00 in binary, the "Two 32-bit acceptance filters" pattern filter is used because there are two bank.

Assume you use 11 bits standard pattern, I think you can use the following pattern for the first/second bank:

pastedImage_1.png

If you use 29 bits extended ID, you can use the following pattern for first/second bank:

pastedImage_3.png

I copy the figure from RM of MC56F80x, they are all use MSCAN, the patten is the same.

Hope it can help you.

BR

Xiangjun Rong

View solution in original post

0 Kudos
Reply
5 Replies
2,074 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Emilio,

As you have read section  32.4.5 Identifier acceptance filter in the RM of KEA128, the MACAN receiver is a 5 stage FIFO instead of separate message buffers, there is only one address space for the receiver FIFO, the actual message ID which is received by MSCAN is saved in MSCAN_REIDR0~3 for 29 bits extended ID and MSCAN_REIDR0~1 for 11 bits standard ID.

Regarding the acceptance of filter, there are two bank: fisrt bank and second bank.

The first bank includes the following registers:

MSCAN_CANIDAR0~3

MSCAN_CANIDMR0~3

The second bank includes the following registers:

MSCAN_CANIDAR4~7

MSCAN_CANIDMR4~7

The IDAM bits in MSCAN_CANIDAC define the filter pattern, I copy it here:

"

Identifier Acceptance Mode

The CPU sets these flags to define the identifier acceptance filter organization.

In filter closed mode, no message is accepted such that the foreground buffer is never reloaded.

00 Two 32-bit acceptance filters.

01 Four 16-bit acceptance filters.

10 Eight 8-bit acceptance filters.

11 Filter closed.

"

Assume that you set the IDAM bits as 00 in binary, the "Two 32-bit acceptance filters" pattern filter is used because there are two bank.

Assume you use 11 bits standard pattern, I think you can use the following pattern for the first/second bank:

pastedImage_1.png

If you use 29 bits extended ID, you can use the following pattern for first/second bank:

pastedImage_3.png

I copy the figure from RM of MC56F80x, they are all use MSCAN, the patten is the same.

Hope it can help you.

BR

Xiangjun Rong

0 Kudos
Reply
2,073 Views
emilioaronmoyer
Contributor III

Hi Xiangjun,

For example if I only what to pass the messages with the ID 0x55 (standard id), waht do I need to put in the first bank registers (

MSCAN_CANIDAR0~3,MSCAN_CANIDMR0~3)?

Regards,

Emilio

0 Kudos
Reply
2,073 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Emilio,

The MSCAN_IDARx register and the MSCAN_RSIDRx register match each other, if you set the received ID as 0x55(the ID bits is 000 0101 0101), and set the IDAM bits as 00, you can set as following:

MSCAN_CANIDAR0=0x0C; //it include ID10~3

MSCAN_CANIDAR1=0xC0  //it includes ID2~0

You can set the MSCAN_CANIDMR0=0xFF; MSCAN_CANIDMR1=0xF8;

It is okay.

Hope it can help you.

BR

XiangJun Rong

0 Kudos
Reply
1,869 Views
Arun5
Contributor I

Hii

  • Can you explain the logic behind this masking, its not clear please provide explanation with other examples
0 Kudos
Reply
2,073 Views
julianmauricioe
Contributor I

Hi Xiangjun, with this configuration:

MSCAN_CANIDAR0=0x0C; //it include ID10~3

MSCAN_CANIDAR1=0xC0  //it includes ID2~0

MSCAN_CANIDMR0=0xFF; MSCAN_CANIDMR1=0xF8;

¿which id wold pass the filter? I dont understad the logical operation. In this example:

id          0000 1010 101

dar        0000 1100 1100

dmr       1111  1111  1111

i dont understand, why id 0x55 pass the filter?

Regards,

Julian echeverry

0 Kudos
Reply