playback any mp4 video from MMC at a resolution of 1024x768 @50 Hz  on i.MX6-SOLO .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

playback any mp4 video from MMC at a resolution of 1024x768 @50 Hz  on i.MX6-SOLO .

590 Views
nagamaheshg
Contributor III

Our main requirement was to playback any mp4 video from MMC at a resolution of 1024x768 @50 Hz  on i.MX6-SOLO .

 

  We tried to play the MP4 video with different resolutions.

  When we played MP4 video with 720 x 480 resolution of 2 min length, the occupied memory is getting free from RAM.

 

  So, we thought playing high resolution video is the issue, as we are  playing 1280*720 resolution of 1.01 hour length video .

But when we played MP4 videos with different resolution of 1 hour length,  we faced the same  issue, but now the memory consumption is slow for  less resolution videos.

 

  Please find the attachment, we checked the memory consumption with free command.

 

$gplay Demo.MP4

is the command which we are giving to play the video

Original Attachment has been moved to: subra_gplay_2.08min.txt.zip

0 Kudos
1 Reply

380 Views
joanxie
NXP TechSupport
NXP TechSupport

I'm not sure what bsp version you use, the below link discuss the mx6 memory leak issue, one can refer to it.

Gstreamer RTMP Streaming Memory Leak In DMA 

https://community.nxp.com/thread/340394 

0 Kudos