Hello Allan,
The file you require is attached. However you probably won't be able to do full chip simulation for this device with your early CW version. Alternatively, you could always remain with the P&E assembler. Since the include file only contains equates, I would expect that it should be compatible with either assembler.
For the latest versions of CW, I believe the memory issue is with the installer program. I have an old Win98 machine with even less memory capacity than yours, and was able to install CW versions 3.1 and 5.0 without problem (except I still have to program the devices using P&E tools). However, for later releases of CW, the normal installation method was problematic. Actually, I have managed, by a round about method, to get CW6.0 at least partially working on this machine.
I also have a WinXP machine on which the later versions will install, but no CW IDE of any version will run at all. But I can still run individual tools alone. What a mess!
Regards,
Mac