deleted
Use Appendix A of the MPCFPE32B.pdf file or Appendix B of the MPC823UM.pdf file.
These files can be loaded using the following links:
http://cache.nxp.com/files/product/doc/MPCFPE32B.pdf?fsrch=1&sr=1&pageNum=1
http://cache.nxp.com/files/product/doc/MPC823UM.pdf?fsrch=1&sr=1&pageNum=1
The "lis" instruction is equivalent to addis rD,0,value instruction.
Definition: Add Immediate Shifted
Operation: if rA = 0 then rD " EXTS(SIMM || (16)0)
else rD " (rA) + EXTS(SIMM || (16)0)
Description: The sum (rA|0) + (SIMM || 0x0000) is placed into rD.
The addis instruction is preferred for addition because it sets few status bits. Note that addis uses the value 0, not the contents of GPR0, if rA = 0.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------