interrupt low time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

interrupt low time

539 Views
amit123
Contributor I

Hi all,

I want to now what is the minimum low time required for PowerPC  interrupt to detect as a valid interrupt.

Pls guide with proper reference.

0 Kudos
Reply
1 Reply

479 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Typically the minimum low time required for PowerPC interrupt to detect as a valid interrupt provided in the data sheet of particular PowerPC device as AC characteristic of its IRQ input. For example the P2020 data sheet (P2020EC) says “when an external interrupt signal is asserted it must remain the assertion for at least 3 system clocks (SYSCLK periods).”

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply