Content originally posted in LPCWare by cstephant on Fri Jun 13 02:35:03 MST 2014
Thanks for the answer.
Both project build configuration are in Debug.
There is no static library dependency and both projects uses Redlib (nohost).
The two disassembled axf are very differents and hard to compare.
It seems that there is a lot of missing steps in fonctions.
For ex:
Good axf :
void xPortSysTickHandler( void )
{
7a4:b580 push{r7, lr}
7a6:b082 subsp, #8
7a8:af00 addr7, sp, #0
unsigned long ulPreviousMask;
Bad axf :
void xPortSysTickHandler( void )
{
5f4:b510 push{r4, lr}
unsigned long ulPreviousMask;
Do you need something else ?