Content originally posted in LPCWare by maxtippy on Tue Jun 25 05:54:45 MST 2013
Hello,
At first, I'm sorry if I ask beginner questions but I haven't any experience with flash programming.
I want to download a simple program and execute into NOR flash on my MCB1800 board with an Lpc1850 on.
The NOR Flash is a Spansion one with the following ref : S29GL064N
For this I find the application note number "11285" about "Writing a flash programming algorithm for unsupported devices" where they provided a flash driver for my board.
I place it into "lpcxpresso_dir/bin/flash" and try to use it.
The download bar went to 100% and they don't report any error. When I check the memory to check if the code is in, it is.
But when the download finished, nothing passed. The code don't execute and I have this message : "No source available for "0x1040683c" "
Is it something specific to do for start execution from NOR Flash ?
I'm using LPCXpresso v.5.2.4 Build 2122 on a Windows 7 64bits, with full licence type.