lpc11xx support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc11xx support?

163 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fentechnt on Mon Dec 14 08:12:22 MST 2009
When will LPCXpresso support the lpc11xx series?  I note that there is now an lpc11xx blinky project available for download from nxp, but it is of little use when the build environment doesn't support the lpc11xx...

I've got a project already started for the 11xx, but may need to decide to move to the lpc13xx instead, if timescales don't fit.
0 Kudos
Reply
1 Reply

155 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Mon Dec 14 11:43:37 MST 2009
An update to LPCXpresso to add LPC11xx support is being tested internally and will be released soon.
0 Kudos
Reply