Content originally posted in LPCWare by akaraivanov on Thu May 17 06:06:54 MST 2012
Thank you!
I checked the RunningOnLinux wiki page and tried to install all required dependencies. There are still some not being installed:
hal-libs.i686
java.i686
libXTrap.i686
opencdk.i686
sane-backends-libs-gphoto2.i686
hal-libs is retired from Fedora 16
java is not found as such. I've fot installed instead:
java-1.7.0-openjdk-1.7.0.3-2.1.fc16.1.i686
libXTrap.i686 is not available in fedora. I installed this old one from the web
libXTrap-1.0.0-4.fc8.i386.rpm
opencdk - not available in F16 installed this package from F14:
opencdk-0.6.6-1400.fc14.i686.rpm
sane-backends-libs-gphoto2.i686 appears to be renamed in F16 to
sane-backends-drivers-cameras-1.0.22-10.fc16.i686
I have SELinux set to permissive.
Despite the additionally installed packages the symptoms have not changed even a bit. I get the IDE hanging when I click on Debug. From this point on, IDE window does not get redrawn if I overlap it with another window. Because of IDE hanging I cannot really follow the procedure for getting the mcu debug log.
In attempt to provide some more information that might reveal anything please find attached in a zip:
- ps of related processes
- pstack run on lpcxpresso process
- pmap of lpcxpresso process
Does anyone have similar setup running on Fedora 16?
Thanks in advance
Alex.
PS: would have been a bit better if the list of dependent packages in RunningOnLinux wiki page does not contain package version numbers as they may differ for different Fedora versions. Most of the packages do not have version number there but there are some that do have it.