Content originally posted in LPCWare by nacrisp on Tue Sep 28 01:17:30 MST 2010
I have an application running on the dev board. It's running fine because it's chattering away on the UART0 and debug LEDs are flashing away, but I can no longer use drag2flash, debug, or mass-erase etc. Essentially I cant connect, with the following error: (jpeg attached)
O2: Failed on connect: Ee(02). Not connected to emulator.
Emu(0): Connected. Was: None. DpID: EDB6. Info RDBV20001
I can drag2flash etc on a colleagues dev board, so is it possible that some settings in my app have affected the serial wire debug?
I have powered up the dev board with the ISP switch depressed and this seems to stop my app running, but it starts up again when I try a drag2flash operation - when I hit switch SW4. - LED1 flashes faster as it should, but LEDS 2-5 are running as per my application.
regards,
Nick