Content originally posted in LPCWare by vtw.433e on Tue May 24 10:19:36 MST 2016 It means your code (and its initialized data) is too large to fit in flash. You will need to change your program to make it fit.
Content originally posted in LPCWare by HammingBird on Tue May 24 02:12:59 MST 2016 Hallo, Thanks for the info.
sorry to say, it doesn't work. I installed the ** Latest version of LPCXpresso IDE : v8.1.4 ** and try to optimize the code, but could not able to remove the error.
the error says, < region 'MFlash4' overflowed by 400 bytes >
I am using the prog "LPC8xx ROM API". you can find it here
Content originally posted in LPCWare by lpcxpresso-support on Mon May 23 05:30:31 MST 2016 This error means that the amount of data (the compiled binary) allocated to the flash called MFlash4 was 280 bytes larger than the size of MFlash4.
Please take a look at the FAQ for further information.