Content originally posted in LPCWare by Patrick_W on Tue Apr 21 01:43:08 MST 2015
Hey R2D2,
1) I changed the capacities Cx1 and Cx2 (7, 10,18, 22 and 33pF) also i changed the crystal (same frequency 14,7456 MHz).
I also changed the board (i got two with the same MCU)
2) I am not completly sure what you mean. But i first used a Sunny crystal unit and then i switched to a Raltron crystal.
3) I am using a LPC1763
4) The attached pictures are meassured on the CLKOUT Pin, but i also meassured on XTAL1 and XTAL2
5) I am using LPCXpresso v7.6.2 with the redlink server and as GDB Debugger: arm-none-eabi-gdb.
6) I tried it on my two different boards, with the same result.
Regards