Content originally posted in LPCWare by eTrig on Fri Mar 28 08:40:24 MST 2014 LPC4370 is a very powerful MCU, but I can't found a demo board. If I want to use this MCU, what is the best way?
Content originally posted in LPCWare by arw on Sun Mar 30 19:08:46 MST 2014 Hello, There are two ways to evaluate this chip. The LPC4370 is designed onto the LPC-Link2 debugger. You can actually use it as a target board for the microcontroller as well, and use one Link2 board to debug another. Also, the oscilloscope/logic analyzer known as LabTool adds additional hardware interfaces to the Link2. The full source code for LabTool is also released. See these sites for details.