Content originally posted in LPCWare by brunoalmeida on Sun Dec 07 12:04:31 MST 2014 Hello,
I've been working with LCP1837 for the last 4 months and i've been facing one problem. Sniffing usb communications from OS (Linux, Mac and Windows) i've notice that they send some request with DataLength bigger than the response. The result is that the code get stuck waiting for the endpoint to be ok, and is impossible to answer this request.
One exemple of request is ModeSens6. The linux PC asks for an answer with 192 length (Wireshark Image).
Content originally posted in LPCWare by gfs_lpc on Wed Dec 10 15:24:34 MST 2014 I'm having the same problem but for another command, INQUIRY with requested data length 255. My board is a host and the device is in a FS bus.