Transfer data from SD card to USB with LPC1768

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Transfer data from SD card to USB with LPC1768

631 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Parsa on Sat Aug 01 09:39:23 MST 2015
Hi friends
I use lpc1768 board and Setting up SD card with RL-FlashFS LIB. now it works correctly .
I also use this example for USB HOST Keil->ARM->Boards->MCB1700->RL->USB->HOST->MSD_File. I can use this demo and USB works correctly too.
Now, I want to copy some text file from SD to USB. In this context, I saw this pagehttps://www.lpcware.com/content/project/Dual-USB-Host-Device-solution?destination=node%252F1106929
I think, I need the operation like that. 
Is it possible? and how much is the rate of transmission?
Thanks for any idea
Labels (1)
0 Kudos
Reply
1 Reply

535 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vahid_22002 on Sun Aug 02 00:14:58 MST 2015
?
0 Kudos
Reply