Content originally posted in LPCWare by ferve on Mon May 25 09:01:02 MST 2015
Hi all!! I'm starting to use LPC1769, and i'm working in a project with a XBEE s2 (DIGI). The problem is that from the XBEE module i'm only receiving the first 16 bytes. I was reading that the problem is that FIFO has only 16 bytes.
Is there a simple way to receive more than 16 bytes???
Here is part of the code:
UARTInit(&uart_var_rx, UART_3, 9600, 8, 'n', 1);
char char_rx[30];
int aux;
for(aux=0;aux<30;aux++)
char_rx[aux] = UARTgetc(&uart_var_rx); //This only receive the first 16 bytes
Thanks!
Fernando