Unable to connect JTAG Jlink -EDU pod to LPC1752

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to connect JTAG Jlink -EDU pod to LPC1752

407 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by newdude on Wed May 11 14:10:24 MST 2016
Feeling embarrassed, but I'm unable to connect my JTAG to my extremely simply derived bare board.  As you'all can see from the attached image, all the appropriate pull ups and pull downs are installed on the JTAG connector. I power up my board and notice the 3.3VDC Vcc is appropriately measured and, as far as I can tell, the LPC1752 is appropriately powered up. I connect my JTAG pod to the connector on the board and proceed to use JLink Commander to determine the state of the MCU. JLink Commander is properly talking to the JTAG pod and requests the type of device and the frequency of the device. The crystal on the board is a 20MHz one, but I'm not sure if that's the frequency of the tap on the MCU side. The default on the JTAG pod side is 4000kHz. JLink Commander states that it is unable to connect. I roll through a few frequencies, to include 20MHz, with no connection obtained.

What am I doing wrong?
Labels (1)
0 Kudos
Reply
1 Reply

383 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply