Content originally posted in LPCWare by rjm on Mon Jan 04 06:59:45 MST 2016 Well, there is some confusion about this. The Manual says that address 0 must be specified and then trigger it. But the user program does not start (both ISP_0 and ISP_1 are high; ISP was started from within the user program using ReinvokeISP();
Addess 4 would contain the reset vector, and that should be written as the start address for the go-command? But then, the manual would present incorrect information.
BTW: in UM10736 (User Manual), the following text presents a false subindex: Quote: Write the start address into [0x5070, 0]. Then trigger the “start application” command by writing the value 0x1 to [0x1F51, 1]. The first sequence should be written as [0x5070, 1].