LPCOpen USB HID class issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCOpen USB HID class issues

579 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by midas on Thu May 30 19:56:33 MST 2013

I have ported the lpcusblib_GenericHidDevice project to my own board, LPC11u37 based. I have encountered a few issues:


1. As an LPCXpresso project it seems to run fine, both with USE_USB_ROM_STACK enabled and disabled, but as an IAR project, when I enable the USE_USB_ROM_STACK flag I get a HardFault exception due to an unaligned access somewhere in the internal rom driver (it does work correctly with this flag disabled, i.e. with the alternative USB drivers in C files)?


2. I wanted to use the EVENT_USB_Device_Connect() and EVENT_USB_Device_Disconnect() routines, but realized nobody ever called them, so they would get optimized away and never fire?


3. I needed to modify the HID descriptors and operation to communicate with the host using EP1 IN and OUT, rather then using reports over EP0. After I modified the original interface descriptor, which only used HID_ReportINEndpoint but no HID_ReportOUTEndpoint, by adding an additional EP in the HID interface descriptors, the HIDClient.exe utility failed to communicate with the application. After digging through the code, I encountered the following remark in file HIDClassDevice.h:


" * @note Due to technical limitations, the HID device class driver does not utilize a separate OUT
 *        endpoint for host->device communications. Instead, the host->device data (if any) is sent to
 *        the device via the control endpoint."
Is that a silicon problem, or a software issue that might get fixed in a future update?

Labels (1)
0 Kudos
0 Replies