Sorry, I've been away for a few days.
Thx for the reply, I did a bit of reading up on you wrote.
The problem is that the flash I want to access is not the boot flash (CS0)
but an additional NAND on the 5329 EVB which is connected to CS2.
I read in another thread that for using a new device with FP,
you have to write a device description (done that) and change
the .cfg file Flash Programmer uses. (done that too)
In there, there are a few lines setting CSAR0 to 0x00000000,
mask and modes, etc. These should activate the CS0 everytime
someone accesses the address space.
I tried to map CSAR2 to 0x10000000, but I found that the instructions
are not carried out. I even commented out all the stuff for CS0 and still
had access to boot flash, so what's set there doesn't seem to matter.
CS0 is boot select, 0x00... is the initial value of CSAR0, so whatever you do,
u get put through to boot flash.
I'm starting a new thread in Codewarrior section about .cfg files.