Exception : Data abort with hcd_hsh1.dll with imx51 evk on wince 6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Exception : Data abort with hcd_hsh1.dll with imx51 evk on wince 6

773 Views
謝端桂
Contributor I

Dear all:

I  use the project solution(iMX51-EVK-Mobility) of imx51 evk bsp.

Sometimes the board boot up, it will show the error message as below:

新增點陣圖影像.bmp

It seems like High speed host 1 error, How do I fix the error and keep the usb function work?

Thank for your help,

Victor

Labels (2)
Tags (1)
0 Kudos
2 Replies

634 Views
igorpadykov
NXP Employee
NXP Employee

Hi Victor

from log seems there are also IPU errors, so issue may be caused

by DDR faults, also recommended to check if ENGcm12051 patch

is implemented:

Updates and Patches (6)

Source code patch to provide SW workaround of erratum ENGcm12051.

Based on the i.MX51 Windows CE 6 1104 release.

i.MX51 Evaluation Kit|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

634 Views
謝端桂
Contributor I

Dear igorpadykov:

I update the source code with the patches, but still get the same problem.

Does any else solutions?

Thanks for your help,

Victor

0 Kudos