Hello, I bought a IMX.6QP SABRE module just a few days ago and there is no
SD card to boot it inside of the pack which is the delivered.
So i am tring to boot it with my personal SD card and i downloaded latest
BSP filse from the internet but i did not succeed it. So please, give me
some advice how i have to do with my personal SD card and windows OS
dekstop.
Thanks.
Hi AUDIN
seems most easy way is to use mfg tools and eMMC, please use
mfgtool2-yocto-mx-sabresd-emmc-6qp.vbs script :
Programmers (Flash, etc.) (2)
IMX6_L4.1.15_MFG_TOOL (REV L4.1.15_1.0.0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------