Are there any guidelines or App Notes to run a T1022 cpu at 600 or 800MHz core clock?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there any guidelines or App Notes to run a T1022 cpu at 600 or 800MHz core clock?

Jump to solution
1,158 Views
Larry5335
Contributor IV

Also power numbers for thermal dissipation.

Labels (1)
0 Kudos
Reply
1 Solution
898 Views
ufedor
NXP Employee
NXP Employee

There is no such application note.

The following requirement has to be fulfilled:

Frequency provided to the e5500 cluster after any dividers must always be greater than or equal to the platform frequency.

View solution in original post

0 Kudos
Reply
5 Replies
899 Views
ufedor
NXP Employee
NXP Employee

There is no such application note.

The following requirement has to be fulfilled:

Frequency provided to the e5500 cluster after any dividers must always be greater than or equal to the platform frequency.

0 Kudos
Reply
898 Views
scottwood
NXP Employee
NXP Employee

Where did you get that requirement?  The documentation I have says that the e5500 cluster frequency must be "greater than half of the platform frequency".

0 Kudos
Reply
898 Views
ufedor
NXP Employee
NXP Employee

QorIQ T1042, T1022 Data Sheet, Rev. 2, Table 129. Processor, platform, and memory clocking specifications, Note 2.

0 Kudos
Reply
898 Views
scottwood
NXP Employee
NXP Employee

I was looking at the note above table 133 in section 4.1.5 of the same document.

0 Kudos
Reply
898 Views
ufedor
NXP Employee
NXP Employee

Response from the Applications Team:

"Note 2 in the Table 129 in section 4.1.2:

“...

Frequency provided to the e5500 cluster after any dividers must always be greater than or equal to the platform frequency.

...”

is correct.

Second note will be corrected in next release of document."

0 Kudos
Reply