Dear Sirs,
I'm starting to develop using KDS 3.2.0, MQX 4.2, KSDK 1.3 with a frdm-k64f board and a PE Micro Multilink universal.
I can compile without issue a couple of demo project (I'm currently focusing on ethernet, so I compiled and run the webserver demo).
The main problem is I cannot compile any c++ source file: I'm using the httpsrc_frdmk64f project as starting point, I added a couple of cpp sources and a couple of hpp headers but these files are simply ignored by KDS. I think that I missing something... Can somebody help me?
Thanks in advance
Alessio
Hello Alessio
You may refer to these blogs to use GCC tool chain with C++:
http://mcuoneclipse.com/2012/10/04/processor-expert-gcc-c-and-kinetis-l-and-mqxlite/
http://mcuoneclipse.com/2014/10/25/c-with-kinetis-design-studio/
Hope this helps!
Best Regards
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------