BLE Attributes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLE Attributes

Jump to solution
1,429 Views
syed_idris
Contributor III

What mean by the Attributes and profiles in BLE ?

Can KW40 communicate to any sensor having bluetooth or it needs special attributes and profiles with sensor ?

Can we send the temperature sensor data from sensor to KW40 by connecting ANY bluetooth device to temperature sensor ?

0 Kudos
Reply
1 Solution
1,102 Views
alexandruandree
NXP Employee
NXP Employee

An attribute is an entity described by type, handle and permissions. Attributes comprise the GATT database. Profiles define specific application behavior.  For further in-depth details, I recommend ATTRIBUTE PROTOCOL chapter and BLUETOOTH PROFILES sub-chapter from the Core specification (Adopted Specifications | Bluetooth Technology Website )

The Temperature sensor and collector implement a custom profile and service. In consequence, temperature data can be retrieved ONLY by a Bluetooth device that implements the same custom profile and a client for the custom service.

View solution in original post

0 Kudos
Reply
1 Reply
1,103 Views
alexandruandree
NXP Employee
NXP Employee

An attribute is an entity described by type, handle and permissions. Attributes comprise the GATT database. Profiles define specific application behavior.  For further in-depth details, I recommend ATTRIBUTE PROTOCOL chapter and BLUETOOTH PROFILES sub-chapter from the Core specification (Adopted Specifications | Bluetooth Technology Website )

The Temperature sensor and collector implement a custom profile and service. In consequence, temperature data can be retrieved ONLY by a Bluetooth device that implements the same custom profile and a client for the custom service.

0 Kudos
Reply